EEO#.SOURCE

Description

This keyword sets the position source used to drive the EEO generator. The position source cannot use the same connector as the EEO connector.

Value

Description

0 None
1 Position Feedback 1 (FB1.P)
2 Position Feedback 2 (FB2.P)
3 Position Feedback 3 (FB3.P)
4 Position Feedback 4 (FB4.P)
5 Position Feedback 5 (FB5.P)
11 Axis 1 Feedback (AXIS1.PL.FB)
12 Axis 2 Feedback (AXIS2.PL.FB)
21 Axis 1 Command (AXIS1.PL.CMD)
22 Axis 2 Command (AXIS2.PL.CMD)

Examples

Code

This command shows the allowed position sources for EEO1. Since EEO1 uses the X23 connector, which FB3 could have used, FB3 is not an allowed source.

-->DRV.HELP EEO1.SOURCE
Help for: EEO1.SOURCE [Integer] [NV] [ReadWrite] [Grouped]
Range: [1, 2, 4, 5]
Default = 1
Actual value = 1

This sets the first EEO instance to use FB2 as the source feedback.

-->EEO1.SOURCE 2

Context

For more information see Output - Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 1 to 5, 11, 12, 21, 22
Default Value 0 (None)
Data Type Integer
See Also  
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

EEO1.SOURCE

4600h

05h

Unsigned8

-

-

Read/Write

No

EEO2.SOURCE

4601h

05h

Unsigned8

-

-

Read/Write

No

EEO3.SOURCE

4603h

05h

Unsigned8

-

-

Read/Write

No

EEO4.SOURCE

4606h

05h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

EEO1.SOURCE

32020

7D14

Unsigned8

Read/Write

-

EEO2.SOURCE

32021

7D15

Unsigned8

Read/Write

-

EEO3.SOURCE

32022

7D16

Unsigned8

Read/Write

-

EEO4.SOURCE

32023

7D17

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

EEO1.SOURCE

32020

Unsigned8

Read/Write

-

EEO2.SOURCE

32021

Unsigned8

Read/Write

-

EEO3.SOURCE

32022

Unsigned8

Read/Write

-

EEO4.SOURCE

32023

Unsigned8

Read/Write

-